4032-T-B1_B_915

Changes compared to the previous version:

V1.1 - 2010.05.06.

Component values in the schematic were modified:
	
	- Value of the LH inductor was changed from 5.6nH to 5.1nH
	- Value of the L0 inductor was changed from 10nH to 12nH

Layout was changed:

	- manuf. notes were updated