4430-T-B1_B_950

Changes compared to the previous version:

V1.1 - 16/06/2010

Component values in the schematic were modified (according to AN436 Rev0.1):
	
	- Value of the RDC resistor was changed from 100R to 120R
	- Value of the L0 inductor was changed from 15nH to 12nH
	- Value of the LM2 inductor was changed from 13nH to 12nH
	- Value of the CM capacitor was changed from 4.3pF to 6.2pF
	- type of Q2 was changed from Jauch to ECS

Layout was changed:

	- manuf. notes were updated


V2.0 - 18/01/2011

General Manufacturing pack update:
	
	- manuf. notes were updated
	- component attributes were updated
	- BOM was updated