4431-T-B1_B_868

Changes compared to the previous version:

V2.0 - 13/01/2011

Component values in the schematic were modified (according to AN436 Rev0.1):
	
	- Value of the RDC resistor was changed from 24R to 47R
	- Value of the LC inductor was changed from 24nH to 100nH
	- Value of the L0 inductor was changed from 24nH to 15nH
	- Value of the LM inductor was changed from 12nH to 9.0nH
	- Value of the CM capacitor was changed from 4.7pF to 8.2pF
	- Value of the CM2 capacitor was changed from 3.3pF to 3.6pF

Layout was modified:
	- Small RF shield can frame was removed
	- Wires were placed from the bottom layer to the top (to increase the shielding effect if the can is mounted).

General Manufacturing pack update:
	
	- type of Q2 was changed from Jauch to ECS
	- manuf. notes were updated
	- component attributes were updated
	- BOM was updated