4431-T-B1_D_434

Changes compared to the previous version:

V2.0 - 13/01/2011

Component values in the schematic were modified (according to AN436 Rev0.1):
	
	- Value of the RDC resistor was changed from 43R to 68R
	- Value of the LC inductor was changed from 100nH to 220nH
	- Value of the L0 inductor was changed from 51nH to 39nH
	- Value of the LM inductor was changed from 36nH to 22nH
	- Value of the LM2 inductor was changed from 16nH to 18nH
	- Value of the C0 capacitor was changed from 3.9pF to 8.2pF
	- Value of the CM capacitor was changed from 3.6pF to 15pF
	- Value of the CM2 capacitor was changed from 6.2pF to 12pF

Layout was modified:
	- Small RF shield can frame was removed
	- Wires were placed from the bottom layer to the top (to increase the shielding effect if the can is mounted).

General Manufacturing pack update:
	
	- type of Q2 was changed from Jauch to ECS
	- manuf. notes were updated
	- component attributes were updated
	- BOM was updated