4432-T-B1_B_915

Changes compared to the previous version:

V1.1 - 16/02/2010

Component values in the schematic were modified:
	
	- Value of the LH inductor was changed from 5.6nH to 5.1nH
	- Value of the L0 inductor was changed from 10nH to 12nH

Layout was changed:

	- Version number was added.

V1.2 - 17/01/2011

Component values in the schematic were modified:
	
	- Value of the CM capacitor was changed from 3.9pF to 3.6pF

Layout was modified:

	- Small RF shield can frame was removed
	- Version number was added

General Manufacturing pack update:
	
	- type of Q2 was changed from Jauch to ECS
	- manuf. notes were updated
	- component attributes were updated
	- BOM was updated