4432-T-B1_D_470

Changes compared to the previous version:

V1.1 - 01/17/2011

General Manufacturing pack update:
	
	- type of Q2 was changed from Jauch to ECS
	- manuf. notes were updated
	- component attributes were updated
	- BOM was updated


V1.2 - 01/11/2012

Component value correction:

	- value of LC was modified from 120nH to 220nH