F330 UART bootloader 
It contains several parts.
* Bootloader firmware 
* PC software application
* Sample user application code
About bootloader real size, we need to check .M51 file 
instead of checking project build result output. The 
reason is there some GAPS interval among vector table. 
Here is the example:
In IDE build output windows, we got code size is 1022 bytes.
Program Size: data=59.0 xdata=512 code=1022
LINK/LOCATE RUN COMPLETE.  0 WARNING(S),  0 ERROR(S)

But check the M51 file, the last function of bootloader locates 
at the last page. This means 0~0x400 are all occupied by bootloader,
So total size of bootloader is:
0x400+size_on_las_page = 0x400 + (0x1C2C - 0x1C00 + 0x13) = 1087 bytes.

            * * * * * * *   C O D E   M E M O R Y   * * * * * * *
            CODE    0000H     0002H     ABSOLUTE     
                    0002H     0001H                  *** GAP ***
            CODE    0003H     0002H     ABSOLUTE     
            CODE    0005H     0004H     UNIT         ?PR?DISABLE_WATCHDOG?F33X_TARGETBL_DEVSPECIFIC
                    0009H     0002H                  *** GAP ***
            CODE    000BH     0002H     ABSOLUTE     
                    000DH     0006H                  *** GAP ***
            CODE    0013H     0002H     ABSOLUTE     
                    0015H     0006H                  *** GAP ***
            CODE    001BH     0002H     ABSOLUTE     
                    001DH     0006H                  *** GAP ***
            CODE    0023H     0002H     ABSOLUTE     
                    0025H     0006H                  *** GAP ***
            CODE    002BH     0002H     ABSOLUTE     
BL51 BANKED LINKER/LOCATER V6.22                                                                  10/15/2014  14:55:47  PAGE 2


                    002DH     0006H                  *** GAP ***
            CODE    0033H     0002H     ABSOLUTE     
                    0035H     0006H                  *** GAP ***
            CODE    003BH     0002H     ABSOLUTE     
            CODE    003DH     000EH     UNIT         ?PR?_SRC_VALIDATE_RESPONSE?FXXX_TARGETBL_MAIN
            CODE    004BH     0002H     ABSOLUTE     
                    004DH     0006H                  *** GAP ***
            CODE    0053H     0002H     ABSOLUTE     
                    0055H     0006H                  *** GAP ***
            CODE    005BH     0002H     ABSOLUTE     
                    005DH     0006H                  *** GAP ***
            CODE    0063H     0002H     ABSOLUTE     
            CODE    0065H     000CH     UNIT         ?PR?DEVICE_INIT?F33X_TARGETBL_DEVSPECIFIC
                    0071H     0002H                  *** GAP ***
            CODE    0073H     0002H     ABSOLUTE     
            CODE    0075H     00E3H     UNIT         ?PR?MAIN?FXXX_TARGETBL_MAIN
            CODE    0158H     0085H     UNIT         ?C_C51STARTUP
            CODE    01DDH     0041H     UNIT         ?PR?_TGT_WRITE_FLASH?FXXX_TARGETBL_COMMANDS
            CODE    021EH     003BH     UNIT         ?C?LIB_CODE
            CODE    0259H     0037H     UNIT         ?PR?_GET_BUF_CRC?F33X_CRC
            CODE    0290H     002DH     UNIT         ?PR?_SRC_GET_PAGE?F33X_COMM_UART
            CODE    02BDH     0028H     UNIT         ?PR?_FLASH_MODIFY?F33X_FLASH
            CODE    02E5H     0024H     UNIT         ?PR?_UPDATE_CRC?F33X_CRC
            CODE    0309H     0023H     UNIT         ?PR?_UART_RECEIVE?F33X_COMM_UART
            CODE    032CH     001EH     UNIT         ?PR?SRC_GET_PAGE_INFO?F33X_COMM_UART
            CODE    034AH     001CH     UNIT         ?PR?_UART_SEND?F33X_COMM_UART
            CODE    0366H     001BH     UNIT         ?PR?_SRC_VALIDATE_PAGECRC?FXXX_TARGETBL_MAIN
            CODE    0381H     001BH     UNIT         ?PR?SRC_DISP_TGT_INFO?F33X_COMM_UART
            CODE    039CH     001BH     UNIT         ?PR?_SRC_DISP_INFO_CODE?F33X_COMM_UART
            CODE    03B7H     0019H     UNIT         ?PR?SRC_GET_INFO?F33X_COMM_UART
            CODE    03D0H     0018H     UNIT         ?PR?UART0_INIT?F33X_TARGETBL_DEVSPECIFIC
            CODE    03E8H     0012H     UNIT         ?PR?F33X_COMM_UART
                    03FAH     1806H                  *** GAP ***
            CODE    1C00H     0010H     UNIT         ?PR?PORT_INIT?F33X_TARGETBL_DEVSPECIFIC
            CODE    1C10H     000AH     UNIT         ?C_INITSEG
            CODE    1C1AH     000AH     UNIT         ?PR?OSCILLATOR_INIT?F33X_TARGETBL_DEVSPECIFIC
            CODE    1C24H     0008H     UNIT         ?PR?_TGT_ERASE_PAGE?FXXX_TARGETBL_COMMANDS
                    1C2CH     00BFH                  *** GAP ***
            CODE    1CEBH     0013H     UNIT         ?CO?FXXX_TARGETBL_INFOBLOCK