Peripheral control example.

This example project use EFM32 CMSIS and the emlib peripheral library to
demonstrate how to enable the access to various on-board peripherals. To
reduce leakage current, the EFM32LG-DK3650 board has several analog switches, and to
enable extended functionality there are multiplexers which need to be
configured correctly for most of the kit peripherals.

The on-board LEDs will light up according to the configured state of the
peripherals.

Board:  Silicon Labs EFM32LG-DK3650 Development Kit
Device: EFM32LG990F256