Nandflash example.

This example demonstrates use of the NANDFLASH driver.

Connect a terminal to the TTL-level serialport (115200-N-8-1) on EXP port pins
4 and 6.
Operations on the flash are initiated by issuing commands on the terminal.
Command "h" will print a help screen on the terminal :

    Available commands:
        fi         : Show NAND flash device information
        h          : Show this help
        rp <n>     : Read page <n>
        bp <n>     : Blankcheck page <n>
        bd         : Blankcheck entire device
        bb         : Check bad-block info
        mb <n>     : Mark block <n> as bad
        wp <n>     : Write page <n>
        eb <n>     : Erase block <n>
        ecc <n>    : Check ECC algorithm, uses page <n> and <n+1>
        cp <m> <n> : Copy page <m> to page <n>

Note that the nandflash device used on this kit has 32 pages per block, so
pages 0-31 belongs to block 0.

Board:  Silicon Labs EFM32LG-STK3600 Development Kit
Device: EFM32LG990F256