Select a single energy mode, and stay there.

This example project uses the EFM32 emlib and demonstrates the use of the LCD 
controller, RTC (real time counter), GPIO and various Energy Modes (EM).

The user can press the pushbuttons PB0 and PB1 to select which energy mode to 
demonstrate.

This demo application has been made to give a quick demo of the
energyAware Profiler from Silicon Labs and to reproduce the different 
energy modes seen in the EFM32 datasheet current consumption table. 

Board:  Silicon Labs EFM32TG_STK3300 Development Kit
Device: EFM32TG840F32