Biometric Demo using the Biometric Sensor add-on board on the EFM32WG-STK3800.

This example project uses the EFM32 CMSIS including emlib and the
board support package support functions/drivers to demonstrate driving
the LCD display on the EFM32WG_STK3800 kit. In addition, it demonstrates the 
use of Silicon Labs I2C based sensors on the expansion board header.

You must have a Silicon Labs Biometric Sensor add-on board to make use of this demo.
Once the demo is started, push button PB0 to change what is displayed. While
on the heart rate monitor display hold your finger on the proximity sensor to 
measure heart rate.

Board:  Silicon Labs EFM32WG-STK3800 Starter Kit and Sensor Add-on board
Device: EFM32WG990F256