GLIB example using the Sharp Memory LCD on the EFM32ZG-STK3200.

This example project uses the GLIB library and the DISPLAY device driver
together with EFM32 CMSIS including EMLIB and board support package support
functions/drivers to demonstrate driving the Sharp Memory LCD display on
the EFM32ZG_STK3200 kit.

The user can switch trough different GLIB example screens by pushing the PB1 button.
The user can reset the demo by pushing the PB0 button.

Board:  Silicon Labs EFM32ZG-STK3200 Development Kit
Device: EFM32ZG222F32