GLIB example using the Sharp Memory LCD on the SLSTK3400A-EFM32HG.

This example project uses the GLIB library and the DISPLAY device driver
together with EFM32 CMSIS including EMLIB and board support package support
functions/drivers to demonstrate driving the Sharp Memory LCD display on
the SLSTK3400A_EFM32HG kit.

The user can switch trough different GLIB example screens by pushing the PB1 button.
The user can reset the demo by pushing the PB0 button.

Board:  Silicon Labs SLSTK3400A-EFM32HG Development Kit
Device: EFM32HG322F64