GLIB example using the Sharp Memory LCD on the SLSTK3401A.

This example project uses the GLIB library and the DISPLAY device driver
together with EFM32 CMSIS including emlib and board support package support
functions/drivers to demonstrate driving the Sharp Memory LCD display on
the SLSTK3401A kit.

The user can switch trough different GLIB example screens by pushing the PB1 button.
The user can reset the demo by pushing the PB0 button.

Board:  Silicon Labs SLSTK3401A Starter Kit
Device: EFM32PG1B200F256