Humidity and temperature demo using the on-board si7021 sensor on the
SLWSTK6221A_EZR32WG board.

This example project uses CMSIS including emlib and the
board support package support functions/drivers to demonstrate driving
the Sharp Memory LCD display and the si7021 humidity and temperature sensor on the
SLWSTK6221A_EZR32WG board.

Board:  Silicon Labs SLWSTK6221A_EZR32WG starter kit.
Device: EZR32WG330F256R55