================ Revision history ============================================
5.0.0:
 - Update to use em_core instead of em_int to implement critical regions.
 - Removed iprintf usage since nanolib is now used by default.

4.4.0:
 - No changes.

4.3.1:
 - No changes.

4.3.0:
 - Implemented USB remote wakeup when usb peripheral is in partial power down
   mode.
 - Fixed usb state error when exiting SUSPENDED state after a remote wakeup.

4.2.1:
 - No changes.

4.2.0:
 - No changes.

4.1.1:
 - Extended USB bus reset duration.
 - Extended USB bus reset recovery time in host stack to be more robust when
   devices are attached.

4.1.0:
 - Fixed bug in host stack, USBH_SetAltInterfaceB() specified device instead
   of interface.

4.0.0:
 - Added support for isochronous endpoint transfers.

3.20.14:
 - Added support for Happy Gecko USB Low Energy Modes (LEM).

3.20.13:
 - No changes.

3.20.12:
 - Replaced USB_EP0_SIZE and USB_MAX_EP_SIZE macros with new versions which
   have correct values for low speed/full speed/endpoint types.

3.20.10:
 - Added support for Happy Gecko USB LEM (Low Energy Modes).
 - Fixed bug in suspend powersave mode implementation.

3.20.9:
 - Added support for Happy Gecko USB peripheral.
 - Improved USB cable plug/unplug robustness.

3.20.7:
 - Fixed bug in device stack when resuming from partial powerdown mode.
 - Disable PHY pins and stop USB clocks in USBD_Stop() and USBH_Stop() functions.
 - Fixed max FIFO size limit for device mode.
 - Fixed possible deadlock in USBD_Init() and USBH_WaitForDeviceConnectionB().
 - Added configurable VBUSEN pin usage to support hw without VBUS switch.

3.20.6:
 - No changes.

3.20.5:
 - Fixed bug which could cause malfunctioning when prescaling core clock.
 - Updated license terms.
 - Fixed potential EP sram partitioning problems.
 - Allow 64 and 32 byte EP0 max packetsize.
 - Fixed bug in USBTIMER_Start(), added check on timeout value of 0.
 - Fixed setting USB device state on USB reset from suspend.
 - Added support for composite devices in the device stack.
 - Made special provisions for passing USB-IF "Powered Suspend" test.

3.20.2:
 - Increased robustness when plug/unplug-ing the USB cable rapidly.
 - Changed implementation of usb string macro, wchar_t is no longer used.
   GCC commandline options -fwide-exec-charset=UTF-16LE, -fshort-wchar and
   -Wl,--no-wchar-size-warning are no longer needed.
   Old version was used like this:
     STATIC_CONST_STRING_DESC( iManufacturer, L"Energy Micro AS" );
   New version is used like this:
     STATIC_CONST_STRING_DESC( iManufacturer, 'E','n','e','r','g','y',' ', \
                                              'M','i','c','r','o',' ','A','S' );

3.20.0:
 - Documentation changes only.

3.0.3:
 - Fixed compile time error when using USB stack energy saving on devices with
   no endpoints in addition to EP0.
 - Fixed bug when repeatedly unplugging/replugging a device USB cable and using
   energy saving modes.

3.0.2:
 - Bugfix: USBD_Init() may now be called when USB peripheral is in partial
   powerdown mode.
 - New function USBD_EpIsBusy( int epAddr ) added to API.
 - Changed USBD_AbortTransfer() from USBD_AbortTransfer( uint8_t ) to
   USBD_AbortTransfer( int ).
 - Added configuration of which hw TIMER the stack will use.

3.0.1:
 - USBD_Stop() now disables all USB related interrupts correctly.
 - Minor documentation changes.
 - Added more flexibility for taking advantage of energymodes in USB applications.
 - Fixed bug in device stack partial powerdown procedure.

3.0.0:
 - Updated to CMSIS_V3, "efm32lib" is now called "emlib"
 - This library has been renamed from "efm32usb" to "usb"
 - Prefixes changed from efm32_ to em_, to reflect changes in emlib
 - Updated software license, see top of every file for details

2.4.1:
 - Corrected USBC clock enable for header file updates

2.4.0:
 - Added raw transfer API in the host USB stack for internal testing purposes.
 - Added USB energy-saving modes in device protocol stack.

2.3.2:
 - 19/12-2011: MSD updates

2.3.0:
 - 29/11-2011: Initial version of host stack.
 - 11/11-2011: Added Doxygen doc for host stack.

2.2.2:
 - 18/10-2011: Fixed bug in USBDHAL_AbortEpOut() which in some scenarios would hang.
 - 18/10-2011: Added function USBD_Stop(), which disables device stack operation.

2.2.1:
 - 23/03-2011: Initial version.
 - 15/04-2011: Added host device stack.
 - 24/05-2011: First release candidate.
 - 06/06-2011: Host driver port plug/unplug code improvements
 - 18/08-2011: Redesign of device abort transfer function.