Micriµm

µC/LIB - Release Notes

Collapse all Expand all
Version 1.37.01

Release date : 2012-12-17

Requirements

  • µC/CPU V1.29.01 or more recent.

New features & improvements

  • Improved argument checking for Mem_HeapGetSizeRem() and Mem_PoolBlkGetUsedAtIx().

API Changes

  • Configuration for the module must now be done in file lib_cfg.h instead of app_cfg.h

Bug fixes

  • Corrected a possible misaligned copy in Mem_Move().
Version 1.37.00

Release date : 2012-05-25

Requirements

  • µC/CPU V1.29.01 or more recent.

New features & improvements

  • Added function Str_Char_Replace() to find and replace a character in a string.
  • Added function Mem_Move() to move data within a buffer with proper overlap management.
  • Error codes are now an enumeration.

API Changes

  • N/A

Bug fixes

  • Fixed bug in Mem_PoolBlkGetUsedAtIx() and Mem_PoolBlkIxGet() that was incorrectly validating the index.
Previous versions

See uC-LIB-ReleaseNotesArchive.pdf for previous versions release notes.