uC/OS-II, The Real-Time Kernel
                                DISTRIBUTION

                              Version  2.92.07

                                READ ME FILE


******************************************************************************
******************************* LICENSING TERMS ******************************
******************************************************************************

Even if C/OS-II is provided in source form, C/OS-II is NOT freeware NOR open 
source software. You are NOT allowed to distribute the source code for C/OS-II 
without written consent from Micrim.

You need to obtain an 'Object Code Distribution License' to embed C/OS-II in 
a product that is sold with the intent to make a profit or, if the product is 
not used for education or 'peaceful' research. 

You need to contact Micrim for licensing details.

******************************************************************************
****************************** TABLE OF CONTENTS *****************************
******************************************************************************

1) Reporting problems
2) Software Upgrades
3) Release Notes

/*$PAGE*/
******************************************************************************
***************************** REPORTING PROBLEMS *****************************
******************************************************************************

    If  you find a problem (i.e. bug) in uC/OS-II, do not hesitate  to  report 
the problem to either:

 1) By email:

    support@micrium.com

 
 2) By writing to us at:

        Micrium
        1290 Weston Road, Suite 306
        Weston, FL 33326
        U.S.A.


 2) By calling Micrium:

        (954) 217-2036
        (954) 217-2037, FAX

    Make sure that the problem you are  reporting is in  uC/OS-II and not your
application.    If you in fact discover a bug in uC/OS-II, check the  uC/OS-II 
web site for a list of known bugs and their fixes:

    www.Micrium.com

    If you are  using  an  older  version,  you should  first  get the lastest
version.  

/*$PAGE*/
******************************************************************************
****************************** SOFTWARE UPGRADES *****************************
******************************************************************************

    As you can see, I have been trying to support uC/OS (i.e. V1.xx) and  now,
uC/OS-II.  When bugs are found, I do my best to promptly correct them.   It is 
virtually  impossible  to notify  everybody that  purchased the code (i.e. the 
diskette)  to  tell  them  that  a  new  version  is  available.    You should 
occasionally check the uC/OS-II WEB site (www.ucos-ii.com) or the  Micrium web
site (www.Micrium.com) to see what version is currently shipping.

    I will not be  upgrading the  publisher  everytime  I add new  features to
uC/OS-II.

    I  would  highly  suggest that you resist changing the  STYLE  of the code
unless you don't mind spending many hours doing so everytime you upgrade.

/*$PAGE*/
******************************************************************************
********************************  RELEASE NOTES  *****************************
******************************************************************************

1) RELEASE NOTES:
----------------
   The release notes are now provided in PDF format in the file:

    \Micrium\Software\uCOS-II\Doc\ReleaseNotes.PDF


2) FEATURES SINCE V2.00:
-----------------------
   All the features added since V2.00 are described in the PDF file:

    \Micrium\Software\uCOS-II\Doc\WhatsNewSince-V200.PDF


3) QUICK REFERENCE CHART:
------------------------
   A Quick Reference Chart for all the functions in V2.9x is provided in the 
   following .PDF files:

    \Micrium\Software\uCOS-II\Doc\QuickRefChart-Color.PDF

   If you have a LAMINATION machine, you can protect the chart by laminating it.


4) REFERENCE AND CONFIGURATION MANUALS:
--------------------------------------
   The updated Reference and Configuration Manual (Chapter 16 and 17 in the 
   MicroC/OS-II 2nd Edition book) have been included in .PDF format in this 
   distribution.  These documents are found in:

    \Micrium\Software\uCOS-II\Doc\uCOS-II-RefMan.PDF   (Chapter 16)
    \Micrium\Software\uCOS-II\Doc\uCOS-II-CfgMan.PDF   (Chapter 17)