![]() |
Energy Micro IEC60355 Library Project 1.037 GCC-Version
IEC60355 Library documentation and API
|
This page explains how to interpret the graphs that are generated by doxygen.
Consider the following example:
/*! Invisible class because of truncation */ class Invisible { }; /*! Truncated class, inheritance relation is hidden */ class Truncated : public Invisible { }; /* Class not documented with doxygen comments */ class Undocumented { }; /*! Class that is inherited using public inheritance */ class PublicBase : public Truncated { }; /*! A template class */ template<class T> class Templ { }; /*! Class that is inherited using protected inheritance */ class ProtectedBase { }; /*! Class that is inherited using private inheritance */ class PrivateBase { }; /*! Class that is used by the Inherited class */ class Used { }; /*! Super class that inherits a number of other classes */ class Inherited : public PublicBase, protected ProtectedBase, private PrivateBase, public Undocumented, public Templ<int> { private: Used *m_usedClass; };
This will result in the following graph:
The boxes in the above graph have the following meaning:
The arrows have the following meaning: