![]() |
Energy Micro IEC60355 Library Project 1.037 GCC-Version
IEC60355 Library documentation and API
|
typedef for a critical floating point variable with 64 bits. More...
#include "iec60335_class_b_critical_data.h"
Data Fields | |
| double | inverse |
| double | data |
typedef for a critical floating point variable with 64 bits.
This variable has to be checked with the macro IEC60335_ClassB_CriticalDataValidate(criticalVar)
Definition at line 59 of file iec60335_class_b_critical_data.h.
| double critical_double_struct::data |
Data content of the critical variable
Definition at line 62 of file iec60335_class_b_critical_data.h.
The complement of the data content of the critical variable
Definition at line 61 of file iec60335_class_b_critical_data.h.