![]() |
Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions
|
#include "efm32g890f128.h"
Data Fields | |
| __IO uint32_t | CTRL |
| __IO uint32_t | CMD |
| __I uint32_t | STATUS |
| __IO uint32_t | IEN |
| __I uint32_t | IF |
| __IO uint32_t | IFS |
| __IO uint32_t | IFC |
| __IO uint32_t | DATA |
| __IO uint32_t | XORDATA |
| uint32_t | RESERVED0 [3] |
| __IO uint32_t | KEYLA |
| __IO uint32_t | KEYLB |
| __IO uint32_t | KEYLC |
| __IO uint32_t | KEYLD |
| __IO uint32_t | KEYHA |
| __IO uint32_t | KEYHB |
| __IO uint32_t | KEYHC |
| __IO uint32_t | KEYHD |
Definition at line 319 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::CMD |
Command Register
Definition at line 322 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::CTRL |
Control Register
Definition at line 321 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::DATA |
DATA Register
Definition at line 328 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::IEN |
Interrupt Enable Register
Definition at line 324 of file efm32g890f128.h.
| __I uint32_t AES_TypeDef::IF |
Interrupt Flag Register
Definition at line 325 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 327 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 326 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::KEYHA |
KEY High Register
Definition at line 335 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::KEYHB |
KEY High Register
Definition at line 336 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::KEYHC |
KEY High Register
Definition at line 337 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::KEYHD |
KEY High Register
Definition at line 338 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::KEYLA |
KEY Low Register
Definition at line 331 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::KEYLB |
KEY Low Register
Definition at line 332 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::KEYLC |
KEY Low Register
Definition at line 333 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::KEYLD |
KEY Low Register
Definition at line 334 of file efm32g890f128.h.
| uint32_t AES_TypeDef::RESERVED0[3] |
Reserved for future use
Definition at line 330 of file efm32g890f128.h.
| __I uint32_t AES_TypeDef::STATUS |
Status Register
Definition at line 323 of file efm32g890f128.h.
| __IO uint32_t AES_TypeDef::XORDATA |
XORDATA Register
Definition at line 329 of file efm32g890f128.h.