Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions

CALIBRATE_TypeDef Struct Reference

#include "efm32g890f128.h"

Data Fields

__I uint32_t ADDRESS
__I uint32_t VALUE

Detailed Description

Definition at line 845 of file efm32g890f128.h.


Field Documentation

Address of calibration register

Definition at line 847 of file efm32g890f128.h.

Default value for calibration register

Definition at line 848 of file efm32g890f128.h.


The documentation for this struct was generated from the following file: