![]() |
Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions
|
#include "efm32g890f128.h"
Data Fields | |
| __IO uint32_t | CTRL |
| __IO uint32_t | HFCORECLKDIV |
| __IO uint32_t | HFPERCLKDIV |
| __IO uint32_t | HFRCOCTRL |
| __IO uint32_t | LFRCOCTRL |
| __IO uint32_t | AUXHFRCOCTRL |
| __IO uint32_t | CALCTRL |
| __IO uint32_t | CALCNT |
| __IO uint32_t | OSCENCMD |
| __IO uint32_t | CMD |
| __IO uint32_t | LFCLKSEL |
| __I uint32_t | STATUS |
| __I uint32_t | IF |
| __IO uint32_t | IFS |
| __IO uint32_t | IFC |
| __IO uint32_t | IEN |
| __IO uint32_t | HFCORECLKEN0 |
| __IO uint32_t | HFPERCLKEN0 |
| uint32_t | RESERVED0 [2] |
| __I uint32_t | SYNCBUSY |
| __IO uint32_t | FREEZE |
| __IO uint32_t | LFACLKEN0 |
| uint32_t | RESERVED1 [1] |
| __IO uint32_t | LFBCLKEN0 |
| uint32_t | RESERVED2 [1] |
| __IO uint32_t | LFAPRESC0 |
| uint32_t | RESERVED3 [1] |
| __IO uint32_t | LFBPRESC0 |
| uint32_t | RESERVED4 [1] |
| __IO uint32_t | PCNTCTRL |
| __IO uint32_t | LCDCTRL |
| __IO uint32_t | ROUTE |
| __IO uint32_t | LOCK |
Definition at line 277 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::AUXHFRCOCTRL |
AUXHFRCO Control Register
Definition at line 284 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::CALCNT |
Calibration Counter Register
Definition at line 286 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::CALCTRL |
Calibration Control Register
Definition at line 285 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::CMD |
Command Register
Definition at line 288 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::CTRL |
CMU Control Register
Definition at line 279 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::FREEZE |
Freeze Register
Definition at line 299 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::HFCORECLKDIV |
High Frequency Core Clock Division Register
Definition at line 280 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::HFCORECLKEN0 |
High Frequency Core Clock Enable Register 0
Definition at line 295 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::HFPERCLKDIV |
High Frequency Peripheral Clock Division Register
Definition at line 281 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::HFPERCLKEN0 |
High Frequency Peripheral Clock Enable Register 0
Definition at line 296 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::HFRCOCTRL |
HFRCO Control Register
Definition at line 282 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::IEN |
Interrupt Enable Register
Definition at line 294 of file efm32g890f128.h.
| __I uint32_t CMU_TypeDef::IF |
Interrupt Flag Register
Definition at line 291 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 293 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 292 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::LCDCTRL |
LCD Control Register
Definition at line 309 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::LFACLKEN0 |
Low Frequency A Clock Enable Register 0 (Async Reg)
Definition at line 300 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::LFAPRESC0 |
Low Frequency A Prescaler Register 0 (Async Reg)
Definition at line 304 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::LFBCLKEN0 |
Low Frequency B Clock Enable Register 0 (Async Reg)
Definition at line 302 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::LFBPRESC0 |
Low Frequency B Prescaler Register 0 (Async Reg)
Definition at line 306 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::LFCLKSEL |
Low Frequency Clock Select Register
Definition at line 289 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::LFRCOCTRL |
LFRCO Control Register
Definition at line 283 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::LOCK |
Configuration Lock Register
Definition at line 311 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::OSCENCMD |
Oscillator Enable/Disable Command Register
Definition at line 287 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::PCNTCTRL |
PCNT Control Register
Definition at line 308 of file efm32g890f128.h.
| uint32_t CMU_TypeDef::RESERVED0[2] |
Reserved for future use
Definition at line 297 of file efm32g890f128.h.
| uint32_t CMU_TypeDef::RESERVED1[1] |
Reserved for future use
Definition at line 301 of file efm32g890f128.h.
| uint32_t CMU_TypeDef::RESERVED2[1] |
Reserved for future use
Definition at line 303 of file efm32g890f128.h.
| uint32_t CMU_TypeDef::RESERVED3[1] |
Reserved for future use
Definition at line 305 of file efm32g890f128.h.
| uint32_t CMU_TypeDef::RESERVED4[1] |
Reserved for future use
Definition at line 307 of file efm32g890f128.h.
| __IO uint32_t CMU_TypeDef::ROUTE |
I/O Routing Register
Definition at line 310 of file efm32g890f128.h.
| __I uint32_t CMU_TypeDef::STATUS |
Status Register
Definition at line 290 of file efm32g890f128.h.
| __I uint32_t CMU_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 298 of file efm32g890f128.h.