![]() |
Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions
|
#include "efm32g890f128.h"
Data Fields | |
| __IO uint32_t | CTRL |
| __I uint32_t | STATUS |
| __IO uint32_t | CH0CTRL |
| __IO uint32_t | CH1CTRL |
| __IO uint32_t | IEN |
| __I uint32_t | IF |
| __IO uint32_t | IFS |
| __IO uint32_t | IFC |
| __IO uint32_t | CH0DATA |
| __IO uint32_t | CH1DATA |
| __IO uint32_t | COMBDATA |
| __IO uint32_t | CAL |
| __IO uint32_t | BIASPROG |
Definition at line 679 of file efm32g890f128.h.
| __IO uint32_t DAC_TypeDef::BIASPROG |
Bias Programming Register
Definition at line 693 of file efm32g890f128.h.
| __IO uint32_t DAC_TypeDef::CAL |
Calibration Register
Definition at line 692 of file efm32g890f128.h.
| __IO uint32_t DAC_TypeDef::CH0CTRL |
Channel 0 Control Register
Definition at line 683 of file efm32g890f128.h.
| __IO uint32_t DAC_TypeDef::CH0DATA |
Channel 0 Data Register
Definition at line 689 of file efm32g890f128.h.
| __IO uint32_t DAC_TypeDef::CH1CTRL |
Channel 1 Control Register
Definition at line 684 of file efm32g890f128.h.
| __IO uint32_t DAC_TypeDef::CH1DATA |
Channel 1 Data Register
Definition at line 690 of file efm32g890f128.h.
| __IO uint32_t DAC_TypeDef::COMBDATA |
Combined Data Register
Definition at line 691 of file efm32g890f128.h.
| __IO uint32_t DAC_TypeDef::CTRL |
Control Register
Definition at line 681 of file efm32g890f128.h.
| __IO uint32_t DAC_TypeDef::IEN |
Interrupt Enable Register
Definition at line 685 of file efm32g890f128.h.
| __I uint32_t DAC_TypeDef::IF |
Interrupt Flag Register
Definition at line 686 of file efm32g890f128.h.
| __IO uint32_t DAC_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 688 of file efm32g890f128.h.
| __IO uint32_t DAC_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 687 of file efm32g890f128.h.
| __I uint32_t DAC_TypeDef::STATUS |
Status Register
Definition at line 682 of file efm32g890f128.h.