![]() |
Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions
|
#include "efm32g890f128.h"

Data Fields | |
| __I uint32_t | STATUS |
| __O uint32_t | CONFIG |
| __IO uint32_t | CTRLBASE |
| __I uint32_t | ALTCTRLBASE |
| __I uint32_t | CHWAITSTATUS |
| __O uint32_t | CHSWREQ |
| __IO uint32_t | CHUSEBURSTS |
| __O uint32_t | CHUSEBURSTC |
| __IO uint32_t | CHREQMASKS |
| __O uint32_t | CHREQMASKC |
| __IO uint32_t | CHENS |
| __O uint32_t | CHENC |
| __IO uint32_t | CHALTS |
| __O uint32_t | CHALTC |
| __IO uint32_t | CHPRIS |
| __O uint32_t | CHPRIC |
| uint32_t | RESERVED0 [3] |
| __IO uint32_t | ERRORC |
| uint32_t | RESERVED1 [880] |
| __I uint32_t | CHREQSTATUS |
| uint32_t | RESERVED2 [1] |
| __I uint32_t | CHSREQSTATUS |
| uint32_t | RESERVED3 [121] |
| __I uint32_t | IF |
| __IO uint32_t | IFS |
| __IO uint32_t | IFC |
| __IO uint32_t | IEN |
| uint32_t | RESERVED4 [60] |
| DMA_CH_TypeDef | CH [8] |
Definition at line 432 of file efm32g890f128.h.
| __I uint32_t DMA_TypeDef::ALTCTRLBASE |
Channel Alternate Control Data Base Pointer Register
Definition at line 437 of file efm32g890f128.h.
Channel registers
Definition at line 465 of file efm32g890f128.h.
| __O uint32_t DMA_TypeDef::CHALTC |
Channel Alternate Clear Register
Definition at line 447 of file efm32g890f128.h.
| __IO uint32_t DMA_TypeDef::CHALTS |
Channel Alternate Set Register
Definition at line 446 of file efm32g890f128.h.
| __O uint32_t DMA_TypeDef::CHENC |
Channel Enable Clear Register
Definition at line 445 of file efm32g890f128.h.
| __IO uint32_t DMA_TypeDef::CHENS |
Channel Enable Set Register
Definition at line 444 of file efm32g890f128.h.
| __O uint32_t DMA_TypeDef::CHPRIC |
Channel Priority Clear Register
Definition at line 449 of file efm32g890f128.h.
| __IO uint32_t DMA_TypeDef::CHPRIS |
Channel Priority Set Register
Definition at line 448 of file efm32g890f128.h.
| __O uint32_t DMA_TypeDef::CHREQMASKC |
Channel Request Mask Clear Register
Definition at line 443 of file efm32g890f128.h.
| __IO uint32_t DMA_TypeDef::CHREQMASKS |
Channel Request Mask Set Register
Definition at line 442 of file efm32g890f128.h.
| __I uint32_t DMA_TypeDef::CHREQSTATUS |
Channel Request Status
Definition at line 453 of file efm32g890f128.h.
| __I uint32_t DMA_TypeDef::CHSREQSTATUS |
Channel Single Request Status
Definition at line 455 of file efm32g890f128.h.
| __O uint32_t DMA_TypeDef::CHSWREQ |
Channel Software Request Register
Definition at line 439 of file efm32g890f128.h.
| __O uint32_t DMA_TypeDef::CHUSEBURSTC |
Channel Useburst Clear Register
Definition at line 441 of file efm32g890f128.h.
| __IO uint32_t DMA_TypeDef::CHUSEBURSTS |
Channel Useburst Set Register
Definition at line 440 of file efm32g890f128.h.
| __I uint32_t DMA_TypeDef::CHWAITSTATUS |
Channel Wait on Request Status Register
Definition at line 438 of file efm32g890f128.h.
| __O uint32_t DMA_TypeDef::CONFIG |
DMA Configuration Register
Definition at line 435 of file efm32g890f128.h.
| __IO uint32_t DMA_TypeDef::CTRLBASE |
Channel Control Data Base Pointer Register
Definition at line 436 of file efm32g890f128.h.
| __IO uint32_t DMA_TypeDef::ERRORC |
Bus Error Clear Register
Definition at line 451 of file efm32g890f128.h.
| __IO uint32_t DMA_TypeDef::IEN |
Interrupt Enable register
Definition at line 461 of file efm32g890f128.h.
| __I uint32_t DMA_TypeDef::IF |
Interrupt Flag Register
Definition at line 458 of file efm32g890f128.h.
| __IO uint32_t DMA_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 460 of file efm32g890f128.h.
| __IO uint32_t DMA_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 459 of file efm32g890f128.h.
| uint32_t DMA_TypeDef::RESERVED0[3] |
Reserved for future use
Definition at line 450 of file efm32g890f128.h.
| uint32_t DMA_TypeDef::RESERVED1[880] |
Reserved for future use
Definition at line 452 of file efm32g890f128.h.
| uint32_t DMA_TypeDef::RESERVED2[1] |
Reserved for future use
Definition at line 454 of file efm32g890f128.h.
| uint32_t DMA_TypeDef::RESERVED3[121] |
Reserved for future use
Definition at line 457 of file efm32g890f128.h.
| uint32_t DMA_TypeDef::RESERVED4[60] |
Reserved registers
Definition at line 463 of file efm32g890f128.h.
| __I uint32_t DMA_TypeDef::STATUS |
DMA Status Registers
Definition at line 434 of file efm32g890f128.h.