Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions

EMU_TypeDef Struct Reference

#include "efm32g890f128.h"

Data Fields

__IO uint32_t CTRL
__IO uint32_t MEMCTRL
__IO uint32_t LOCK
uint32_t RESERVED0 [6]
__IO uint32_t AUXCTRL

Detailed Description

Definition at line 250 of file efm32g890f128.h.


Field Documentation

__IO uint32_t EMU_TypeDef::AUXCTRL

Auxiliary Control Register

Definition at line 257 of file efm32g890f128.h.

__IO uint32_t EMU_TypeDef::CTRL

Control Register

Definition at line 252 of file efm32g890f128.h.

__IO uint32_t EMU_TypeDef::LOCK

Configuration Lock Register

Definition at line 254 of file efm32g890f128.h.

__IO uint32_t EMU_TypeDef::MEMCTRL

Memory Control Register

Definition at line 253 of file efm32g890f128.h.

Reserved for future use

Definition at line 256 of file efm32g890f128.h.


The documentation for this struct was generated from the following file: