Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions

GPIO_TypeDef Struct Reference

#include "efm32g890f128.h"

Collaboration diagram for GPIO_TypeDef:

Data Fields

GPIO_P_TypeDef P [6]
uint32_t RESERVED0 [10]
__IO uint32_t EXTIPSELL
__IO uint32_t EXTIPSELH
__IO uint32_t EXTIRISE
__IO uint32_t EXTIFALL
__IO uint32_t IEN
__I uint32_t IF
__IO uint32_t IFS
__IO uint32_t IFC
__IO uint32_t ROUTE
__IO uint32_t INSENSE
__IO uint32_t LOCK

Detailed Description

Definition at line 377 of file efm32g890f128.h.


Field Documentation

__IO uint32_t GPIO_TypeDef::EXTIFALL

External Interrupt Falling Edge Trigger Register

Definition at line 385 of file efm32g890f128.h.

__IO uint32_t GPIO_TypeDef::EXTIPSELH

External Interrupt Port Select High Register

Definition at line 383 of file efm32g890f128.h.

__IO uint32_t GPIO_TypeDef::EXTIPSELL

External Interrupt Port Select Low Register

Definition at line 382 of file efm32g890f128.h.

__IO uint32_t GPIO_TypeDef::EXTIRISE

External Interrupt Rising Edge Trigger Register

Definition at line 384 of file efm32g890f128.h.

__IO uint32_t GPIO_TypeDef::IEN

Interrupt Enable Register

Definition at line 386 of file efm32g890f128.h.

__I uint32_t GPIO_TypeDef::IF

Interrupt Flag Register

Definition at line 387 of file efm32g890f128.h.

__IO uint32_t GPIO_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 389 of file efm32g890f128.h.

__IO uint32_t GPIO_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 388 of file efm32g890f128.h.

__IO uint32_t GPIO_TypeDef::INSENSE

Input Sense Register

Definition at line 392 of file efm32g890f128.h.

__IO uint32_t GPIO_TypeDef::LOCK

Configuration Lock Register

Definition at line 393 of file efm32g890f128.h.

Port configuration bits

Definition at line 379 of file efm32g890f128.h.

Reserved for future use

Definition at line 381 of file efm32g890f128.h.

__IO uint32_t GPIO_TypeDef::ROUTE

I/O Routing Register

Definition at line 391 of file efm32g890f128.h.


The documentation for this struct was generated from the following file: