Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions

LETIMER_TypeDef Struct Reference

#include "efm32g890f128.h"

Data Fields

__IO uint32_t CTRL
__IO uint32_t CMD
__I uint32_t STATUS
__I uint32_t CNT
__IO uint32_t COMP0
__IO uint32_t COMP1
__IO uint32_t REP0
__IO uint32_t REP1
__I uint32_t IF
__IO uint32_t IFS
__IO uint32_t IFC
__IO uint32_t IEN
__IO uint32_t FREEZE
__I uint32_t SYNCBUSY
uint32_t RESERVED0 [2]
__IO uint32_t ROUTE

Detailed Description

Definition at line 579 of file efm32g890f128.h.


Field Documentation

__IO uint32_t LETIMER_TypeDef::CMD

Command Register

Definition at line 582 of file efm32g890f128.h.

__I uint32_t LETIMER_TypeDef::CNT

Counter Value Register

Definition at line 584 of file efm32g890f128.h.

__IO uint32_t LETIMER_TypeDef::COMP0

Compare Value Register 0

Definition at line 585 of file efm32g890f128.h.

__IO uint32_t LETIMER_TypeDef::COMP1

Compare Value Register 1

Definition at line 586 of file efm32g890f128.h.

__IO uint32_t LETIMER_TypeDef::CTRL

Control Register

Definition at line 581 of file efm32g890f128.h.

__IO uint32_t LETIMER_TypeDef::FREEZE

Freeze Register

Definition at line 594 of file efm32g890f128.h.

__IO uint32_t LETIMER_TypeDef::IEN

Interrupt Enable Register

Definition at line 592 of file efm32g890f128.h.

__I uint32_t LETIMER_TypeDef::IF

Interrupt Flag Register

Definition at line 589 of file efm32g890f128.h.

__IO uint32_t LETIMER_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 591 of file efm32g890f128.h.

__IO uint32_t LETIMER_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 590 of file efm32g890f128.h.

__IO uint32_t LETIMER_TypeDef::REP0

Repeat Counter Register 0

Definition at line 587 of file efm32g890f128.h.

__IO uint32_t LETIMER_TypeDef::REP1

Repeat Counter Register 1

Definition at line 588 of file efm32g890f128.h.

Reserved for future use

Definition at line 597 of file efm32g890f128.h.

__IO uint32_t LETIMER_TypeDef::ROUTE

I/O Routing Register

Definition at line 598 of file efm32g890f128.h.

Status Register

Definition at line 583 of file efm32g890f128.h.

Synchronization Busy Register

Definition at line 595 of file efm32g890f128.h.


The documentation for this struct was generated from the following file: