![]() |
Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions
|
#include "efm32g890f128.h"
Data Fields | |
| __IO uint32_t | CTRL |
| __IO uint32_t | CMD |
| __I uint32_t | STATUS |
| __IO uint32_t | CLKDIV |
| __IO uint32_t | STARTFRAME |
| __IO uint32_t | SIGFRAME |
| __I uint32_t | RXDATAX |
| __I uint32_t | RXDATA |
| __I uint32_t | RXDATAXP |
| __IO uint32_t | TXDATAX |
| __IO uint32_t | TXDATA |
| __I uint32_t | IF |
| __IO uint32_t | IFS |
| __IO uint32_t | IFC |
| __IO uint32_t | IEN |
| __IO uint32_t | PULSECTRL |
| __IO uint32_t | FREEZE |
| __I uint32_t | SYNCBUSY |
| uint32_t | RESERVED0 [3] |
| __IO uint32_t | ROUTE |
Definition at line 548 of file efm32g890f128.h.
| __IO uint32_t LEUART_TypeDef::CLKDIV |
Clock Control Register
Definition at line 553 of file efm32g890f128.h.
| __IO uint32_t LEUART_TypeDef::CMD |
Command Register
Definition at line 551 of file efm32g890f128.h.
| __IO uint32_t LEUART_TypeDef::CTRL |
Control Register
Definition at line 550 of file efm32g890f128.h.
| __IO uint32_t LEUART_TypeDef::FREEZE |
Freeze Register
Definition at line 567 of file efm32g890f128.h.
| __IO uint32_t LEUART_TypeDef::IEN |
Interrupt Enable Register
Definition at line 564 of file efm32g890f128.h.
| __I uint32_t LEUART_TypeDef::IF |
Interrupt Flag Register
Definition at line 561 of file efm32g890f128.h.
| __IO uint32_t LEUART_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 563 of file efm32g890f128.h.
| __IO uint32_t LEUART_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 562 of file efm32g890f128.h.
| __IO uint32_t LEUART_TypeDef::PULSECTRL |
Pulse Control Register
Definition at line 565 of file efm32g890f128.h.
| uint32_t LEUART_TypeDef::RESERVED0[3] |
Reserved for future use
Definition at line 570 of file efm32g890f128.h.
| __IO uint32_t LEUART_TypeDef::ROUTE |
I/O Routing Register
Definition at line 571 of file efm32g890f128.h.
| __I uint32_t LEUART_TypeDef::RXDATA |
Receive Buffer Data Register
Definition at line 557 of file efm32g890f128.h.
| __I uint32_t LEUART_TypeDef::RXDATAX |
Receive Buffer Data Extended Register
Definition at line 556 of file efm32g890f128.h.
| __I uint32_t LEUART_TypeDef::RXDATAXP |
Receive Buffer Data Extended Peek Register
Definition at line 558 of file efm32g890f128.h.
| __IO uint32_t LEUART_TypeDef::SIGFRAME |
Signal Frame Register
Definition at line 555 of file efm32g890f128.h.
| __IO uint32_t LEUART_TypeDef::STARTFRAME |
Start Frame Register
Definition at line 554 of file efm32g890f128.h.
| __I uint32_t LEUART_TypeDef::STATUS |
Status Register
Definition at line 552 of file efm32g890f128.h.
| __I uint32_t LEUART_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 568 of file efm32g890f128.h.
| __IO uint32_t LEUART_TypeDef::TXDATA |
Transmit Buffer Data Register
Definition at line 560 of file efm32g890f128.h.
| __IO uint32_t LEUART_TypeDef::TXDATAX |
Transmit Buffer Data Extended Register
Definition at line 559 of file efm32g890f128.h.