Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions

MSC_TypeDef Struct Reference

#include "efm32g890f128.h"

Data Fields

__IO uint32_t CTRL
__IO uint32_t READCTRL
__IO uint32_t WRITECTRL
__IO uint32_t WRITECMD
__IO uint32_t ADDRB
uint32_t RESERVED0 [1]
__IO uint32_t WDATA
__I uint32_t STATUS
uint32_t RESERVED1 [3]
__I uint32_t IF
__IO uint32_t IFS
__IO uint32_t IFC
__IO uint32_t IEN
__IO uint32_t LOCK

Detailed Description

Definition at line 225 of file efm32g890f128.h.


Field Documentation

__IO uint32_t MSC_TypeDef::ADDRB

Page Erase/Write Address Buffer

Definition at line 231 of file efm32g890f128.h.

__IO uint32_t MSC_TypeDef::CTRL

Memory System Control Register

Definition at line 227 of file efm32g890f128.h.

__IO uint32_t MSC_TypeDef::IEN

Interrupt Enable Register

Definition at line 241 of file efm32g890f128.h.

__I uint32_t MSC_TypeDef::IF

Interrupt Flag Register

Definition at line 238 of file efm32g890f128.h.

__IO uint32_t MSC_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 240 of file efm32g890f128.h.

__IO uint32_t MSC_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 239 of file efm32g890f128.h.

__IO uint32_t MSC_TypeDef::LOCK

Configuration Lock Register

Definition at line 242 of file efm32g890f128.h.

__IO uint32_t MSC_TypeDef::READCTRL

Read Control Register

Definition at line 228 of file efm32g890f128.h.

Reserved for future use

Definition at line 233 of file efm32g890f128.h.

Reserved for future use

Definition at line 237 of file efm32g890f128.h.

__I uint32_t MSC_TypeDef::STATUS

Status Register

Definition at line 235 of file efm32g890f128.h.

__IO uint32_t MSC_TypeDef::WDATA

Write Data Register

Definition at line 234 of file efm32g890f128.h.

__IO uint32_t MSC_TypeDef::WRITECMD

Write Command Register

Definition at line 230 of file efm32g890f128.h.

__IO uint32_t MSC_TypeDef::WRITECTRL

Write Control Register

Definition at line 229 of file efm32g890f128.h.


The documentation for this struct was generated from the following file: