Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions

PCNT_TypeDef Struct Reference

#include "efm32g890f128.h"

Data Fields

__IO uint32_t CTRL
__IO uint32_t CMD
__I uint32_t STATUS
__I uint32_t CNT
__I uint32_t TOP
__IO uint32_t TOPB
__I uint32_t IF
__IO uint32_t IFS
__IO uint32_t IFC
__IO uint32_t IEN
__IO uint32_t ROUTE
__IO uint32_t FREEZE
__I uint32_t SYNCBUSY

Detailed Description

Definition at line 606 of file efm32g890f128.h.


Field Documentation

__IO uint32_t PCNT_TypeDef::CMD

Command Register

Definition at line 609 of file efm32g890f128.h.

__I uint32_t PCNT_TypeDef::CNT

Counter Value Register

Definition at line 611 of file efm32g890f128.h.

__IO uint32_t PCNT_TypeDef::CTRL

Control Register

Definition at line 608 of file efm32g890f128.h.

__IO uint32_t PCNT_TypeDef::FREEZE

Freeze Register

Definition at line 620 of file efm32g890f128.h.

__IO uint32_t PCNT_TypeDef::IEN

Interrupt Enable Register

Definition at line 617 of file efm32g890f128.h.

__I uint32_t PCNT_TypeDef::IF

Interrupt Flag Register

Definition at line 614 of file efm32g890f128.h.

__IO uint32_t PCNT_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 616 of file efm32g890f128.h.

__IO uint32_t PCNT_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 615 of file efm32g890f128.h.

__IO uint32_t PCNT_TypeDef::ROUTE

I/O Routing Register

Definition at line 618 of file efm32g890f128.h.

__I uint32_t PCNT_TypeDef::STATUS

Status Register

Definition at line 610 of file efm32g890f128.h.

__I uint32_t PCNT_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 621 of file efm32g890f128.h.

__I uint32_t PCNT_TypeDef::TOP

Top Value Register

Definition at line 612 of file efm32g890f128.h.

__IO uint32_t PCNT_TypeDef::TOPB

Top Value Buffer Register

Definition at line 613 of file efm32g890f128.h.


The documentation for this struct was generated from the following file: