![]() |
Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions
|
PRS_CH. More...
#include "efm32g890f128.h"
Data Fields | |
| __IO uint32_t | CTRL |
PRS_CH.
Definition at line 399 of file efm32g890f128.h.
| __IO uint32_t PRS_CH_TypeDef::CTRL |
Channel Control Register
Definition at line 401 of file efm32g890f128.h.