![]() |
Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions
|
#include "efm32g890f128.h"

Data Fields | |
| __IO uint32_t | SWPULSE |
| __IO uint32_t | SWLEVEL |
| uint32_t | RESERVED0 [2] |
| PRS_CH_TypeDef | CH [8] |
Definition at line 409 of file efm32g890f128.h.
Channel registers
Definition at line 416 of file efm32g890f128.h.
| uint32_t PRS_TypeDef::RESERVED0[2] |
Reserved registers
Definition at line 414 of file efm32g890f128.h.
| __IO uint32_t PRS_TypeDef::SWLEVEL |
Software Level Register
Definition at line 412 of file efm32g890f128.h.
| __IO uint32_t PRS_TypeDef::SWPULSE |
Software Pulse Register
Definition at line 411 of file efm32g890f128.h.