Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions

RMU_TypeDef Struct Reference

#include "efm32g890f128.h"

Data Fields

__IO uint32_t CTRL
__I uint32_t RSTCAUSE
__O uint32_t CMD

Detailed Description

Definition at line 265 of file efm32g890f128.h.


Field Documentation

__O uint32_t RMU_TypeDef::CMD

Command Register

Definition at line 269 of file efm32g890f128.h.

__IO uint32_t RMU_TypeDef::CTRL

Control Register

Definition at line 267 of file efm32g890f128.h.

__I uint32_t RMU_TypeDef::RSTCAUSE

Reset Cause Register

Definition at line 268 of file efm32g890f128.h.


The documentation for this struct was generated from the following file: