Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions

ROMTABLE_TypeDef Struct Reference

#include "efm32g890f128.h"

Data Fields

__I uint32_t PID4
__I uint32_t PID5
__I uint32_t PID6
__I uint32_t PID7
__I uint32_t PID0
__I uint32_t PID1
__I uint32_t PID2
__I uint32_t PID3
__I uint32_t CID0

Detailed Description

Definition at line 825 of file efm32g890f128.h.


Field Documentation

__I uint32_t ROMTABLE_TypeDef::CID0

Unused

Definition at line 835 of file efm32g890f128.h.

__I uint32_t ROMTABLE_TypeDef::PID0

Chip family LSB, chip major revision

Definition at line 831 of file efm32g890f128.h.

__I uint32_t ROMTABLE_TypeDef::PID1

JEP_106_NO, Chip family MSB

Definition at line 832 of file efm32g890f128.h.

__I uint32_t ROMTABLE_TypeDef::PID2

Chip minor rev MSB, JEP_106_PRESENT, JEP_106_NO

Definition at line 833 of file efm32g890f128.h.

__I uint32_t ROMTABLE_TypeDef::PID3

Chip minor rev LSB

Definition at line 834 of file efm32g890f128.h.

__I uint32_t ROMTABLE_TypeDef::PID4

JEP_106_BANK

Definition at line 827 of file efm32g890f128.h.

__I uint32_t ROMTABLE_TypeDef::PID5

Unused

Definition at line 828 of file efm32g890f128.h.

__I uint32_t ROMTABLE_TypeDef::PID6

Unused

Definition at line 829 of file efm32g890f128.h.

__I uint32_t ROMTABLE_TypeDef::PID7

Unused

Definition at line 830 of file efm32g890f128.h.


The documentation for this struct was generated from the following file: