![]() |
Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions
|
#include "efm32g890f128.h"
Data Fields | |
| __IO uint32_t | CTRL |
| __I uint32_t | CNT |
| __IO uint32_t | COMP0 |
| __IO uint32_t | COMP1 |
| __I uint32_t | IF |
| __IO uint32_t | IFS |
| __IO uint32_t | IFC |
| __IO uint32_t | IEN |
| __IO uint32_t | FREEZE |
| __I uint32_t | SYNCBUSY |
Definition at line 767 of file efm32g890f128.h.
| __I uint32_t RTC_TypeDef::CNT |
Counter Value Register
Definition at line 770 of file efm32g890f128.h.
| __IO uint32_t RTC_TypeDef::COMP0 |
Compare Value Register 0
Definition at line 771 of file efm32g890f128.h.
| __IO uint32_t RTC_TypeDef::COMP1 |
Compare Value Register 1
Definition at line 772 of file efm32g890f128.h.
| __IO uint32_t RTC_TypeDef::CTRL |
Control Register
Definition at line 769 of file efm32g890f128.h.
| __IO uint32_t RTC_TypeDef::FREEZE |
Freeze Register
Definition at line 778 of file efm32g890f128.h.
| __IO uint32_t RTC_TypeDef::IEN |
Interrupt Enable Register
Definition at line 776 of file efm32g890f128.h.
| __I uint32_t RTC_TypeDef::IF |
Interrupt Flag Register
Definition at line 773 of file efm32g890f128.h.
| __IO uint32_t RTC_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 775 of file efm32g890f128.h.
| __IO uint32_t RTC_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 774 of file efm32g890f128.h.
| __I uint32_t RTC_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 779 of file efm32g890f128.h.