Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions

TIMER_CC_TypeDef Struct Reference

TIMER_CC. More...

#include "efm32g890f128.h"

Data Fields

__IO uint32_t CTRL
__IO uint32_t CCV
__I uint32_t CCVP
__IO uint32_t CCVB

Detailed Description

TIMER_CC.

Definition at line 471 of file efm32g890f128.h.


Field Documentation

__IO uint32_t TIMER_CC_TypeDef::CCV

CC Channel Value Register

Definition at line 474 of file efm32g890f128.h.

__IO uint32_t TIMER_CC_TypeDef::CCVB

CC Channel Buffer Register

Definition at line 476 of file efm32g890f128.h.

__I uint32_t TIMER_CC_TypeDef::CCVP

CC Channel Value Peek Register

Definition at line 475 of file efm32g890f128.h.

__IO uint32_t TIMER_CC_TypeDef::CTRL

CC Channel Control Register

Definition at line 473 of file efm32g890f128.h.


The documentation for this struct was generated from the following file: