Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions

TIMER_TypeDef Struct Reference

#include "efm32g890f128.h"

Collaboration diagram for TIMER_TypeDef:

Data Fields

__IO uint32_t CTRL
__IO uint32_t CMD
__I uint32_t STATUS
__IO uint32_t IEN
__I uint32_t IF
__IO uint32_t IFS
__IO uint32_t IFC
__IO uint32_t TOP
__IO uint32_t TOPB
__IO uint32_t CNT
__IO uint32_t ROUTE
uint32_t RESERVED0 [1]
TIMER_CC_TypeDef CC [3]
uint32_t RESERVED1 [4]
__IO uint32_t DTCTRL
__IO uint32_t DTTIME
__IO uint32_t DTFC
__IO uint32_t DTOGEN
__I uint32_t DTFAULT
__O uint32_t DTFAULTC
__IO uint32_t DTLOCK

Detailed Description

Definition at line 484 of file efm32g890f128.h.


Field Documentation

Compare/Capture Channel

Definition at line 500 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::CMD

Command Register

Definition at line 487 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::CNT

Counter Value Register

Definition at line 495 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::CTRL

Control Register

Definition at line 486 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::DTCTRL

DTI Control Register

Definition at line 503 of file efm32g890f128.h.

__I uint32_t TIMER_TypeDef::DTFAULT

DTI Fault Register

Definition at line 507 of file efm32g890f128.h.

DTI Fault Clear Register

Definition at line 508 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::DTFC

DTI Fault Configuration Register

Definition at line 505 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::DTLOCK

DTI Configuration Lock Register

Definition at line 509 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::DTOGEN

DTI Output Generation Enable Register

Definition at line 506 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::DTTIME

DTI Time Control Register

Definition at line 504 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::IEN

Interrupt Enable Register

Definition at line 489 of file efm32g890f128.h.

__I uint32_t TIMER_TypeDef::IF

Interrupt Flag Register

Definition at line 490 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 492 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 491 of file efm32g890f128.h.

Reserved registers

Definition at line 498 of file efm32g890f128.h.

Reserved for future use

Definition at line 502 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::ROUTE

I/O Routing Register

Definition at line 496 of file efm32g890f128.h.

__I uint32_t TIMER_TypeDef::STATUS

Status Register

Definition at line 488 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::TOP

Counter Top Value Register

Definition at line 493 of file efm32g890f128.h.

__IO uint32_t TIMER_TypeDef::TOPB

Counter Top Value Buffer Register

Definition at line 494 of file efm32g890f128.h.


The documentation for this struct was generated from the following file: