Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions

USART_TypeDef Struct Reference

#include "efm32g890f128.h"

Data Fields

__IO uint32_t CTRL
__IO uint32_t FRAME
__IO uint32_t TRIGCTRL
__IO uint32_t CMD
__I uint32_t STATUS
__IO uint32_t CLKDIV
__I uint32_t RXDATAX
__I uint32_t RXDATA
__I uint32_t RXDOUBLEX
__I uint32_t RXDOUBLE
__I uint32_t RXDATAXP
__I uint32_t RXDOUBLEXP
__IO uint32_t TXDATAX
__IO uint32_t TXDATA
__IO uint32_t TXDOUBLEX
__IO uint32_t TXDOUBLE
__I uint32_t IF
__IO uint32_t IFS
__IO uint32_t IFC
__IO uint32_t IEN
__IO uint32_t IRCTRL
__IO uint32_t ROUTE

Detailed Description

Definition at line 517 of file efm32g890f128.h.


Field Documentation

__IO uint32_t USART_TypeDef::CLKDIV

Clock Control Register

Definition at line 524 of file efm32g890f128.h.

__IO uint32_t USART_TypeDef::CMD

Command Register

Definition at line 522 of file efm32g890f128.h.

__IO uint32_t USART_TypeDef::CTRL

Control Register

Definition at line 519 of file efm32g890f128.h.

__IO uint32_t USART_TypeDef::FRAME

USART Frame Format Register

Definition at line 520 of file efm32g890f128.h.

__IO uint32_t USART_TypeDef::IEN

Interrupt Enable Register

Definition at line 538 of file efm32g890f128.h.

__I uint32_t USART_TypeDef::IF

Interrupt Flag Register

Definition at line 535 of file efm32g890f128.h.

__IO uint32_t USART_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 537 of file efm32g890f128.h.

__IO uint32_t USART_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 536 of file efm32g890f128.h.

__IO uint32_t USART_TypeDef::IRCTRL

IrDA Control Register

Definition at line 539 of file efm32g890f128.h.

__IO uint32_t USART_TypeDef::ROUTE

I/O Routing Register

Definition at line 540 of file efm32g890f128.h.

__I uint32_t USART_TypeDef::RXDATA

RX Buffer Data Register

Definition at line 526 of file efm32g890f128.h.

__I uint32_t USART_TypeDef::RXDATAX

RX Buffer Data Extended Register

Definition at line 525 of file efm32g890f128.h.

RX Buffer Data Extended Peek Register

Definition at line 529 of file efm32g890f128.h.

RX FIFO Double Data Register

Definition at line 528 of file efm32g890f128.h.

RX Buffer Double Data Extended Register

Definition at line 527 of file efm32g890f128.h.

RX Buffer Double Data Extended Peek Register

Definition at line 530 of file efm32g890f128.h.

__I uint32_t USART_TypeDef::STATUS

USART Status Register

Definition at line 523 of file efm32g890f128.h.

__IO uint32_t USART_TypeDef::TRIGCTRL

USART Trigger Control register

Definition at line 521 of file efm32g890f128.h.

__IO uint32_t USART_TypeDef::TXDATA

TX Buffer Data Register

Definition at line 532 of file efm32g890f128.h.

__IO uint32_t USART_TypeDef::TXDATAX

TX Buffer Data Extended Register

Definition at line 531 of file efm32g890f128.h.

__IO uint32_t USART_TypeDef::TXDOUBLE

TX Buffer Double Data Register

Definition at line 534 of file efm32g890f128.h.

__IO uint32_t USART_TypeDef::TXDOUBLEX

TX Buffer Double Data Extended Register

Definition at line 533 of file efm32g890f128.h.


The documentation for this struct was generated from the following file: