Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions

VCMP_TypeDef Struct Reference

#include "efm32g890f128.h"

Data Fields

__IO uint32_t CTRL
__IO uint32_t INPUTSEL
__I uint32_t STATUS
__IO uint32_t IEN
__I uint32_t IF
__IO uint32_t IFS
__IO uint32_t IFC

Detailed Description

Definition at line 718 of file efm32g890f128.h.


Field Documentation

__IO uint32_t VCMP_TypeDef::CTRL

Control Register

Definition at line 720 of file efm32g890f128.h.

__IO uint32_t VCMP_TypeDef::IEN

Interrupt Enable Register

Definition at line 723 of file efm32g890f128.h.

__I uint32_t VCMP_TypeDef::IF

Interrupt Flag Register

Definition at line 724 of file efm32g890f128.h.

__IO uint32_t VCMP_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 726 of file efm32g890f128.h.

__IO uint32_t VCMP_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 725 of file efm32g890f128.h.

__IO uint32_t VCMP_TypeDef::INPUTSEL

Input Selection Register

Definition at line 721 of file efm32g890f128.h.

__I uint32_t VCMP_TypeDef::STATUS

Status Register

Definition at line 722 of file efm32g890f128.h.


The documentation for this struct was generated from the following file: