![]() |
Energy Micro IEC60355 Library Example Project 1.0 (internal use only!) GCC-Version
Example project demonstrating POST and BIST library functions
|
#include "efm32g890f128.h"
Data Fields | |
| __IO uint32_t | CTRL |
| __IO uint32_t | CMD |
| __I uint32_t | SYNCBUSY |
Definition at line 787 of file efm32g890f128.h.
| __IO uint32_t WDOG_TypeDef::CMD |
Command Register
Definition at line 790 of file efm32g890f128.h.
| __IO uint32_t WDOG_TypeDef::CTRL |
Control Register
Definition at line 789 of file efm32g890f128.h.
| __I uint32_t WDOG_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 792 of file efm32g890f128.h.