CP210x Macintosh OSX VCP Driver v2.9 Release Notes Copyright (C) 2011 Silicon Laboratories, Inc. This release contains the following components: * SiLabsUSBDriverDisk.dmg - Image containing the VCP Driver Installer * ReleaseNotes.txt (this file) Known Issues and Limitations ---------------------------- This release includes the Macintosh OSX driver for the Intel and PowerPC Platforms. Driver Installation ------------------- Mount the DMG file and double click the Silicon Labs USB Driver Installer to run the driver installation. Release Dates ------------- CP210x Macintosh OSX VCP Driver v2.9 - May 17, 2011 CP210x Macintosh OSX Driver Revision History -------------------------------------------- Version 2.9 Corrected issue with Baud Rates not being set properly if they were greater than 230400 on PPC or Intel platforms Corrected an issue where a device might get stuck when coming out of sleep mode Corrected an issue on PPC where Baud Rates were not getting set properly Added enhanced support for sleep, now reads state on sleep and writes state on wake to provide smoother and more stable state transitions Version 2.7 Corrected issue with initial Stop Bits value Corrected issue which seen which switching between 32 and 64 bit mode and trying to use the driver in each mode Added in a clear stall to be more complete in invalid control transfers Version 2.6 Corrected all known Kernel Panics for 10.4/5/6 for surprise removal and data transmission Corrected an issue with data drop while using XON/XOFF flow control Corrected RTS/DTR toggling sync issue Version 2.2 Corrected Kernel Panic in Snow Leopard which would randomly occur after transmission Modified DTR pin to toggle on open and close instead of on insertion Modified driver to load without showing the Network Connection Dialog Modified driver to allow toggling of RTS and DTR pins Added 64 bit support for Snow Leopard Version 2.1 Corrected device strings that were changed in the 2.0 release back to the format used in pre-2.0 drivers Version 2.0 Driver architecture updated. Version 1.06 Corrected a bug which causes a Kernel Panic with a Baud Rate of 0, yileding a Divide-By-Zero error Version 1.04 Updated to support newer versions of Mac OSX Version 1.02 Updated to support the Intel platform through a universal binary that also supports PowerPC. Version 1.00 Initial Release