Si4455 revC2A Command/Property API Documentation

Interface Version: 1.0

Document Version: 2.0.5

Generated: 2015-03-18T10:15:42-05:00


Introduction

This document provides API descriptions for the commands and properties used to control and configure the part. The interface version tracks any functional changes to the API (command, property, field, enumeration, etc.). The documentation version tracks any text changes to the summary or description text of the API components.

The commands are listed in a summary table with links to command details. The properties are listed in a summary table with links to property details. The feature available column in the summary tables lists the firmware revision which first implemented the command or property.

An entry in the summary table will link to a details section, which contains a register view with fields. Clicking a field in the register view will auto-expand the corresponding field details. An up button in the field detail links back to the register view. Each register view title links back to the summary table entry. These hyper-links provide two-click access from top to bottom.

Command Summary

BOOT_COMMANDS
Number Name Summary Feature Available
0x02 POWER_UP Command to power-up the device and select the operational mode and functionality.
COMMON_COMMANDS
Number Name Summary Feature Available
0x00 NOP No Operation command.
0x01 PART_INFO Reports basic information about the device.
0x10 FUNC_INFO Returns the Function revision information of the device.
0x44 READ_CMD_BUFF Used to read CTS and the command response.
ADVANCED_COMMANDS
Number Name Summary Feature Available
0x23 GET_CHIP_STATUS Returns the interrupt status of the Chip Interrupt Group (both STATUS and PENDING). Optionally, it may be used to clear latched (PENDING) interrupt events.

Property Summary

Command Details

BOOT_COMMANDS

POWER_UP


COMMON_COMMANDS

NOP


PART_INFO


FUNC_INFO


READ_CMD_BUFF


ADVANCED_COMMANDS

GET_CHIP_STATUS


Property Details