API documentation changes:
v.2.0.4
-	ALL 					Missing pictures of formulas are put back
-	ALL					FUNC_INFO: PATCH reply field is shown
-	EZRadio_REVC2, EZRadioPRO_REVC2		START_TX: TXCOMPLETE_STATE - TX State added
-	EZRadio_REVC2, EZRadioPRO_REVC2		GLOBAL_WUT_CONFIG : WUT_EN field description extended
-	EZRadio_REVC2, EZRadioPRO_REVC2		PTI_LOG_EN description improved
-	EZRadioPRO_REVC2			3 of 6 encoding/decoding (bit EN_3_OF_6 of property PKT_CONFIG2) is added to Si4060-C2, Si4063-C2 and Si4362-C2
-	EZRadioPRO_REVC2			MODEM_DSA_CTRL2:SYNC_QUAL bit is put back
-	EZRadioPRO_REVC2			Argument and reply fields are added to the IRCAL_MANUAL command description
-	EZRadioPRO_REVC2			Default value of MODEM_IFPKD_THRESHOLDS corrected

v.2.0.5
-	ALL					File compression added

API documentation known issues
v.2.0.5
-	EZRadioPRO_REVC2			TX_HOP command is missing from Si4060C2 and Si4063C2 API documentation
-	EZRadioPRO_REVB1			IRCAL_MANUAL command is wrongly present in the document, it is not available in the EZRadioPRO_REVB1 chips