Enter to Win a Metering Development Tool
The Wireless M-Bus demonstration kit is an easy and effective way to demonstrate the low power characteristics of a virtual utility meter running the wireless M-Bus stack.
The right hand side of the demonstration kit acts as a meter that contains a low power C8051F930 MCU, an Si4431 transceiver, and a CP2400 LCD controller. The left hand side of the board is a measurement system that monitors the virtual meter and determines its power consumption.
Using a wireless M-Bus metering application, you can easily adjust parameters of the meter (e.g. message size, RX/TX parameters, etc.) and observe the effect on the real-time power monitor display.
Fill out the fields below to enter to win the Wireless M-Bus Metering development tool. If you are already registered, log in and the fields will be filled out automatically.