QuickSense™ Charge-Timing CDC Sensing Technology
The Silicon Labs patent-pending QuickSense SAR Charge-Timing Capacitance to Digital Converter (CDC) enables the industry’s fastest CDC without sacrificing sensitivity performance.
The unique hardware implementation of the CDC is capable of measuring capacitance on a wide range of materials including the following:
- Printed circuit board
- Flex circuit
- ITO on glass and film
The innovative circuit employs a pair of current sources driving two separate capacitors:
- The CDC’s internal reference capacitor denoted as CREF
- External CSENSOR

The current source denoted as IREF is a fixed current used to drive the CREF capacitor to provide a constant ramp voltage.
The second current source denoted ISENSOR sources a variable current to the sensor capacitor. After each measurement cycle the SAR logic will change the value of ISENSOR, attempting to get the ramp rate the same as the reference capacitor. The circuit also offers a powerful wake-on-touch feature.
Capacitive Touch Sense Overview
Learn how to implement the Charge-Timing Capacitive Sensing technology.
Available Products
* Denotes maximum value in family
** CT denotes Charge-Timing CDC