Human Interface Training and Resources


Videos

QuickSense Portfolio Overview
QuickSense Human Interface Portfolio Overview

Advanced Gesture Recognition
Advanced Gesture Recognition—Go Beyond Touch Sense
Proximity & Ambient Light Sensor Solutions
Proximity & Ambient Light Sensor Solutions
QuickSense Lunar Landing Demo
Touchless Control of Lunar Landing Game
See demo of Si114x infrared multi-function board
Si114x Infrared Multi-Function Board
QuickSense Studio Overview
QuickSense Studio Overview

Back to Top


Web-Based Utilities

IR Range Estimator

This web-based utility will help you determine if the object you're detecting with the Si114x proximity and ambient light sensors will be within range, and if the SNR threshold is high enough to trigger a detection event. This tool can determine if you have adequate SNR in less than a minute.

Optical Sensor Current Estimator

This current estimator utility will help you determine how much current is required for your application. Specify whether you need proximity light sensing, ambient light sensing, or both. Choose your channels, and view the estimated average current results in real time.

Back to Top


White Papers

Designing Intuitive Gesture-Based Human Interface Systems

Unlike human-to-human gesturing, human-machine gesturing does not have a foundation of thousands of years of history to serve as a context and this poses a challenge for human interface system designers. How does a system designer minimize the pain of “learning” gestures for the user?

Capacitive Touch and Proximity Sensing Design Considerations

The availability of enabling technology that can revolutionize the way we interact with consumer electronics products and an urgency to incorporate this technology demonstrates the increased importance consumers are placing on interface design. What defines good human interface design, and how can system designers implement a smarter, friendlier and more intuitive solution?

Touchless Gesturing Brings New Innovation to Electronic Product Design

This in-depth white paper examines how through advancements in human interface (HI) technology and design, infrared proximity sensors are poised to usher in the next user interface paradigm centered on touchless gesturing.

Add Capacitive and Infrared Proximity Sensing to Your Application

Next-generation products require next-generation human interfaces to differentiate themselves in the marketplace, and two of the primary technologies driving this interface development are capacitive and proximity sensing. This white paper addresses the 3 most common challenges when designing human interfaces: power consumption, system responsiveness and interface control.

USB Design Considerations

Choosing the right USB communications option depends on several factors, and each solution has different requirements and degrees of flexibility for both the developer and end-user. Is development of USB firmware or drivers required? Does the end-user need to install a driver? Is a PCB redesign required? How much PCB space is available for additional components? Download this white paper to determine the easiest, most cost-effective way to add USB communications to new designs or a legacy system.

How to Add Gesture Recognition to User Interfaces

Imagine being able to control electronics products at home and in the office, not with a direct touch but with the sweep of your hand. Advanced “touchless” human interface technology is now within the realm of practical implementation, even for products as commonplace as the alarm clock beside your bed. This white paper shows you how you can add touchless gesture interpretation like set and swipe detection to your application.

Low Power Design Using Capacitive Sensing

In many applications, mechanical push button switches and potentiometers are being replaced by capacitive switches, sliders, and control wheels to implement functions such as contrast, volume control, and power on. In this tutorial we’ll explore how to design the user interface of ultra low power applications using capacitive sensing technology, with a specific focus on system definition, hardware design and firmware design.

Back to Top


Presentations

QuickSense™ Touchless Slider Evaluation Kit Demonstration

This step by step video highlights the QuickSense Studio using the Touchless Slider EK. See how quickly and easily you can implement complex gesture.

QuickSense API Demonstration

See a demonstration of the QuickSense API and learn about the structure of the projects created by the QuickSense Configuration Wizard. The demo starts with an overview of the API and makes its way through the files that make up the QuickSense API project for capacitive sensing.

Music Keyboard Demo

This application example uses the Keyboard Evaluation Kit to illustrate the use of capacitive touch sense switches using the C8051F700 family of MCUs with Silicon Labs Capacitance to Digital Converter (CDC) technology.

C8051F990 Slider Demonstration

This video provides a brief introduction to the Silicon Labs capacitance to digital converter and highlights a low power slider implemented with the C8051F990 capacitive touch sense MCU. In addition, the video provides a visual demonstration of the wake-on slide feature and the evaluation kit functions.

C8051F98x/99x Overview

Ultra-low power microcontroller with capacitive touch sense capabilities is now available with the introduction of the C8051F990 MCU. This training module starts with low power principles and specifications and then moves on to an introduction of the Silicon Labs robust capacitance to digital converter and how it is used to implement single and multi-touch gestures via PCB pads. In addition, an application example is provided that shows how to wake an MCU from a low power state using a slider function.

Solutions for Active Infrared Proximity Sensing

Learn the basics of active infrared proximity sensing and the challenges designers face when implementing this technology.  In addition, this course provides an overview of the Si1120 and Si1102 active proximity sensors and walks through a complete 3 LED code example that illustrates how to interface the devices to the Silicon Labs C8051 MCUs.

Capacitive Sensing Technology

Learn about Silicon Labs’ solutions for capacitive sensing in touch applications. This module covers the theory behind the new capacitance to digital converter.

C8051F7xx Overview

Learn about the C8051F70x/71x family designed for human interface capacitive touch sense applications and high pin count designs.

C8051F7xx Capacitive Touch Sense Overview

Learn how to implement capacitance sensing using the C8051F70x/1x family.

The Flexible C8051F7xx High Speed ADC

Learn about the C8051F70x/1x capacitive touch sense family and how to use the analog to digital converter peripheral.

CP240x 128/64 Segment LCD Driver Overview

Learn about the theory and operation of segmented Liquid Crystal Displays (LCD) and how the CP240x family can be used in an ultra low power system to drive the display. In addition to basic theory, the module covers how to connect the display to the IC and how it maps to software as well as covering additional features of the CP204x family.

C8051F7xx SPI Serial Peripheral Interface (SPI) Overview

Learn about the C8051F70x/1x capacitive touch sense and how to implement serial communications using the Enhanced SPI module.

UART Communications

Learn how to implement asynchronous serial communications using the UART peripheral in the C8051F700 capacitive touch sense microcontroller, including the steps required to program the MCU.

C8051F700 SMBus Overview

Learn about the SMBus/I2C and how to implement a two wire interface using the C8051F70x/1x capacitive touch sense.

F700 EEPROM

Learn how to implement low density data storage using the EEPROM peripheral in the C8051F70x/1x MCU.

Back to Top