-------------------------------------------------- Battery Life Estimator v1.20 Release Notes Copyright (C) 2008 Silicon Laboratories, Inc. -------------------------------------------------- This release contains the following components: * BatteryTypes (directory) - Battery description files * DischargeProfiles (directory) - Discharge Profile description files - BatteryLifeEstimator.exe - BatteryLifeEstimator.ini - ReleaseNotes.txt (this file) Release Dates ------------- Battery Life Estimator v1.20 - September 19, 2009 Battery Life Estimator v1.1 - June 26, 2008 Battery Life Estimator v1.0 - February 25, 2008 Revision History ----------------- Version 1.20 Corrections ----------- - Updated Help files. - Changed caption to Silicon Labs battery Life Estimator Version 1.1 New features/Enhancements ------------------------- - Added a help file. - Battery description files now contain a parameter for maximum battery life. Estimated battery life values on the Simulation Results dialog will not exceed this limit. - The minimum system operating voltage limit specified in the discharge profile now works for the single and parallel battery configurations if the starting voltage is greater than the minimum system operating voltage. Version 1.0 New features/Enhancements ------------------------- Initial release. Corrections ----------- Initial release.