After I change the firmware of mcu(C8051F342)  in evb, is there method of restoring the original firmware?

 

  • Audio and Radio
  • Discussion Forums
Unanswered
  • I did not understand your question here.
    are you asking the method to Flash the STK?
    you could flash the MCU on the DK board any firmware you want.
    if you have the original firmware, you could flash it into the MCU any time.

    0
  • I hope I could get the original firmware source.of si4705-d60​-evb.

    I want to restore the original firmware by using its source.

    I would also like to take advantage of the source code on the product being developed.

    Thank you.

    0