Where can I find the si4684 firmware. I'm looking at host loading to start with. With a view to later moving to loading from nvram which I understand requires me to patch the bootloader first.

  • Discussion Forums
  • Audio and Radio
  • Answered
Answered
  • Please download the latest Si468x package from the below link. For host loading, you will need patch + fw image. For flash loading, you will need mini-patch+patch+fw image. For flash loading, host will need to load the mini-patch first.

     

    Download: https://webftp.silabs.com/download?domain=silabs.com&id=t5usMTMJYFpv3m50rPnO-eGDfsvXM4Dnt

    Correct Answer
    0
  • That was more then helpful, thank you very much :-)

    0
  • Link is outdatet. Pls repost.

    TNX,

    /H.

     

    0
  • Dear, as posted before the link is outdated and I couldn't find the complete datasheet and firmware anywhere. Could you please let me know where to download it? Thanks in advance.

    0
  • Please check for actual firmware and datasheets...thanks

    0
  • Hi,

     

    could you post me the firmware and the GUI ?

     

    Thanks !

    0
  • Hello,

     

    could you please repost as wished above?

    The link is not useful anymore.

     

    Full datasheet and firmware is needed !

     

    Best regrads,

    Thomas

    0
  •  


    Thomas1 wrote:

     

    ...

     

    Please look here: http://community.silabs.com/t5/Other-Products/SI4689-firmware/m-p/164054#M427

     

    Best regards,

    Andi

    0
  • Hello again,

     

    thanks for all your help!

    0
  • hi

    i also need the si4684 firmware ,please give me!!1!!

    thanks

    0